SPRAC71C February 2019 – March 2026
Interoperability between toolchains requires that addressing generated by one is consistent with placement generated by another, especially with respect to addressing.
This requires the ABI to establish some conventions. Some of these conventions depend on toolchain-specific behavior, such as code generation models supported, or even user behavior, such as command line options selected or language extensions applied. For this reason, the ABI takes a two-pronged approach:
The toolchain generating the addressing may only have visibility to a variable's declaration and not its definition. Therefore, the conventions must be based only on information available at both points. This excludes, for example, the use of array dimensions.