SPRAC71C February 2019 – March 2026
Attributes that are specified by this ABI are recorded in the subsection with the vendor string C28x. Toolchains should determine compatibility between relocatable files using solely these attributes; vendor-specific information should not be used other than as permitted by the Tag_Compatibility attribute which is provided for this purpose.
The vendor data in the C28x subsection contains any number of attribute vectors. Attribute vectors begin with a scope tag that specifies whether they apply to the entire file or only to listed sections or symbols. An attribute vector has one of the following three formats:

The length field specifies the length in bytes of the entire attribute vector, including the other fields. The symbol and section number fields are sequences of section or symbol indexes, terminated with 0.
Attributes in an attribute vector are represented as a sequence of tag-value pairs. Tags are represented as ULEB128 constants. Values are either ULEB128 constants or NULL-terminated strings.
The effect of omitting a tag in the file scope is identical to including it with a value of 0 or "", depending on the parameter type.
To allow a consumer to skip unrecognized tags, the parameter type is standardized as ULEB128 for even-numbered tags and a NULL-terminated string for odd-numbered tags. Tags 1, 2, 3 (the scope tags) and 32 (Tag_ABI_Compatibility) are exceptions to this convention.
As the ABI evolves, new attributes may be added. To enable older toolchains to robustly process files that may contain attributes they do not comprehend, the ABI adopts the following conventions: