SPRAC71C February 2019 – March 2026
Each EXTAB entry is one or more 32-bit words that encode frame unwinding instructions and descriptors to handle catch and cleanup. The first word describes that entry's personality, which is the format and interpretation of the entry.
When an exception is thrown, EXTAB entries are decoded by “personality routines” provided in the runtime support library. Personality routines specified by the ABI are listed in Table 9-1.