SPRACV1B February 2022 – January 2024 AM2434 , AM6411 , AM6412 , AM6421 , AM6441 , AM6442
This section provides test results and observation for DDR to DDR data copy using UDMA channels.
| Buffer Size (Bytes) |
|
||||
|---|---|---|---|---|---|
| 1 BCDMA Channel | 2 BCDMA Channels | 4 BCDMA Channels | 8 BCDMA Channels | 16 BCDMA Channels | |
| 1 | 1.143 | 1.6 | 2.13 | 2.06 | 1.80 |
| 2 | 5.33 | 6.4 | 5.33 | 4.74 | 3.88 |
| 4 | 8 | 12.8 | 10.67 | 9.85 | 7.88 |
| 8 | 16 | 21.33 | 23.27 | 18.96 | 15.51 |
| 16 | 42.67 | 42.67 | 46.54 | 39.38 | 31.51 |
| 32 | 85.33 | 85.33 | 93.09 | 75.85 | 63.01 |
| 64 | 170.67 | 204.8 | 170.67 | 157.54 | 124.12 |
| 128 | 256 | 341.33 | 341.33 | 341.33 | 282.48 |
| 256 | 512 | 585.14 | 630.15 | 655.36 | 555.39 |
| 512 | 1024 | 1170.28 | 1489.45 | 1424.69 | 1285.02 |
| 1024 | 1638.4 | 2048 | 2730.67 | 2520.61 | 2520.61 |
| 2048 | 2340.57 | 2978.91 | 3640.89 | 4369.07 | 3236.34 |
| 4096 | 3276.8 | 4369.07 | 4681.14 | 5041.23 | 3615.78 |
| 8192 | 4096 | 5698.79 | 4946.11 | 4946.11 | 4017.53 |
| 16384 | 4681.14 | 6898.52 | 5140.08 | 5190.97 | 4136.39 |
| 32768 | 4946.11 | 7710.12 | 5322.72 | 5165.40 | 4181.76 |
Figure 4-6 shows the DDR to DDR read performance curve using BCDMA channels.
The 1 BCDMA channel is being referred to as 1 TRPD.
Data shown here range from 40B to 1600B for clear visualization purpose.
Figure 4-6 DDR Performance GraphObservation:
Maximum throughput is achieved with 4 parallel DMA transfers, further adding of channels will work but will not increase throughput.