SPRACY8 September 2021 TMS320F2800132 , TMS320F2800133 , TMS320F2800135 , TMS320F2800137 , TMS320F2800152-Q1 , TMS320F2800153-Q1 , TMS320F2800154-Q1 , TMS320F2800155 , TMS320F2800155-Q1 , TMS320F2800156-Q1 , TMS320F2800157 , TMS320F2800157-Q1 , TMS320F280025C , TMS320F280033 , TMS320F280034 , TMS320F280034-Q1 , TMS320F280036-Q1 , TMS320F280036C-Q1 , TMS320F280037 , TMS320F280037-Q1 , TMS320F280037C , TMS320F280037C-Q1 , TMS320F280038-Q1 , TMS320F280038C-Q1 , TMS320F280039 , TMS320F280039-Q1 , TMS320F280039C , TMS320F280039C-Q1
A majority of the time, mechanical angular positional sensors obtain the rotor position. Incremental encoders are one of the popular solutions to determine rotor position because they provide high-angular resolution and an accurate derived speed feedback over the whole speed range. These features enable incremental encoders to be frequently used for speed/position control in motor control applications.
Today, many servo motors come with built-in incremental position encoders, commonly referred to as ABZ encoders by the names of their output signals, A, B and I, to feedback the motor-shaft angle once you know the index. Table 3-1 shows the data pins required by the QEP peripheral that should be wired to the corresponding pins on the encoder.
| Pin Type | Pin Name | Pin Usage Per Motor |
|---|---|---|
| Digital | EQEOxA | 3 |
| EQEPxB | ||
| EQEPxI |