SPRADO9 March 2025 AM62L
Fast Fourier Transform (FFT) is one of the most common signal processing algorithms. Table 2-6 shows a 1024-point single precision floating point complex FFT execution time on Arm-Cortex-A53. The benchmark on Arm-Cortex-A53 uses the implementation from Ne10 library, which leverages the Advanced SIMD or NEON acceleration of Cortex-A53. This library is not included in the SDK, but can be downloaded from the official Ne10 repository.
| Arm-Cortex-A53 at 1.25GHz (single thread / core) |
|
|---|---|
| 1024-point Complex FFT execution time | 37µs |