a. AWR_CALIB_MON_TIME_UNIT_CONF_SB Configure runtime calibration/monitoring period
a.1 CALIB_MON_TIME_UNIT is used to configure the minimum periodic unit for completing runtime calibration/monitoring, which is an integer multiple of the frame period
a.2 NUM_OF_CASCADED_DEV Configures the number of cascaded devices. The scope described in this article is 1
a.3 DEVICE_ID The scope described in this article is 0
a.4 MONITORING_MODE The scope described in this article is 0 (default configuration)
b. AWR_RUN_TIME_CALIBRATION_CONF_AND_TRIGGER_SB Configure one-time calibration and runtime calibration
b.1 ONE_TIME_CALIB_ENABLE_MASK: Trigger the corresponding calibration option once based on the flag bits. If other calibrations are still executing, calibration will be performed after the previous calibrations are completed. Calibration takes effect in the frame starting after the asynchronous event is issued
b.2 PERIODIC_CALIB_ENABLE_MASK: Periodically execute calibration items of the corresponding calibration options,
b.3 CALIBRATION_ERIODICITY: The calibration period, which needs to be >= 1s. The unit of the calibration period is the monitoring period, and the calibration results are as described in b.1
b.4 ENABLE_CAL_REPORT: Controls whether calibration results are reported via asynchronous events
b.5 TX_POWER_CAL_MODE: Calibration mode for transmission power
b.6 CAL_TEMP_INDEX_OVERRIDE_ENABLE: Configure the corresponding calibration item to overwrite the calibration value automatically obtained by the chip internally based on temperature with the specified temperature calibration value.
b.7 CAL_TEMP_INDEX_TX Calibration values corresponding to different temperatures for the transmitter module
b.8 CAL_TEMP_INDEX_RX Calibration values corresponding to different temperatures for the receiver module
b.9 CAL_TEMP_INDEX_LODIST Calibration values corresponding to different temperatures for LODIST
b.10 CAL_TEMP_INDEX_TXPHASE Calibration values corresponding to different temperatures for transmission phase
c. AWR_RUN_TIME_CALIBRATION_SUMMARY_REPORT_AE_SB Asynchronous event for runtime calibration results.
c.1 CALIBRATION_ERROR_FLAG Each bit corresponds to the calibration result of a calibration item, where 1 represents pass and 0 represents fail
c.2 CALIBRATION_UPDATE_STATUS Each bit corresponds to whether the calibration item is updated, where 1 represents updated and 0 represents not updated
c.3 TEMPERATURE Calibration temperature
c.4 TIME_STAMP Timestamp of calibration
d. AWR_MONITOR_RF_DIG_LATENTFAULT_CONF_SB Used to configure and detect whether there are potential faults in the digital part of the RF front-end, usually completed before framing because it requires transmitting a specific waveform built into the chip.
d.1 DIG_MONITORING_ENABLES Corresponding digital part detection items
d.2 TEST_MODE Detection mode
e. AWR_MONITOR_RF_DIG_PERIODIC_CONF_SB Used to configure periodic monitoring of whether the digital part of the RF front-end is normal.
e.1 REPORTING_MODE 0 for periodic reporting, 1 for reporting only when an abnormality occurs
e.2 PERIODIC_DIG_MON_EN Corresponding digital part detection items
f. AWR_MONITOR_ANALOG_ENABLES_CONF_SB Used to monitor whether all analog parts are working properly, and completed within one CALIB_MON_TIME_UNIT time.