SPRADU6 October 2026 AWR2944 , AWR2944P
Divided into 3 categories according to whether the monitoring item is susceptible to interference:
Type0: No transmission, causing no interference to other radars.
Type1: Transmission without reception; at this time, the interference has a minor impact on the radar itself, but will affect other radars with reception enabled.
Type2: Both transmission and reception are enabled; interference will be received at this time.
Figure 2-6 Interference Types of Monitoring Functions