SPRADU7 October 2026 AWRL1432
Connect the DCA1000EVM, computer, and AWRL1432BOOST as shown in Figure 5-1, configure the computer's IP address to 192.168.33.30, and then run radar_toolbox_4_00_00_05\tools\Adc_Data_Capture_Tool_DCA1000_CLI|\rawDataCaptureGUI_DCA1000CLI.exe. As shown in Figure 5-2, select the serial port number, cfg file, capture file path, capture duration, etc., in the GUI interface, and click Go to start data capture. The software will automatically issue the cfg file and configure the DCA1000EVM for data capture. Upon completion of data capture, the bin file is stored in the data folder under the current path.
Figure 5-1 Connection Diagram of AWRL1432 and DCA1000
Figure 5-2 Software Interface of rawDataCaptureGUI_DCA1000CLI.exe