SPRSP96B March 2024 – March 2026 TDA4AEN-Q1 , TDA4VEN-Q1
PRODUCTION DATA
This section describes connectivity requirements for package balls that have specific connectivity requirements and unused package balls.
All power pins must be supplied with the voltages specified in Recommended Operating Conditions, unless otherwise specified.
For additional clarification, "leave unconnected" or "no connect" (NC) means no signal traces can be connected to these device ball numbers.
| AMW BALL NUMBER |
BALL NAME | CONNECTION REQUIREMENTS |
|---|---|---|
| B7 B10 |
MCU_ERRORn TRSTn |
Each of these balls must be connected to VSS through separate external pull resistors to ensure these balls are held to a valid logic-low level if a PCB signal trace is connected and not actively driven by an attached device. The internal pull-down can be used to hold a valid logic-low level if no PCB signal trace is connected to the ball. |
| A11 E12 F11 |
TCK TDI TMS |
Each of these balls must be connected to the corresponding power supply(1) through separate external pull resistors to ensure the inputs associated with these balls are held to a valid logic-high level if a PCB signal trace is connected and not actively driven by an attached device. The internal pull-up can be used to hold a valid logic-high level if no PCB signal trace is connected to the ball. |
| C9 F9 D10 E26 E8 B23 B13 E11 B9 D11 F1 J1 U1 T1 |
EMU0 EMU1 MCU_RESETz RESET_REQz MCU_PORz EXTINTN MCU_I2C0_SCL MCU_I2C0_SDA WKUP_I2C0_SCL WKUP_I2C0_SDA DDR0_DQS0_n DDR0_DQS1_n DDR0_DQS2_n DDR0_DQS3_n |
Each of these balls must be connected to the corresponding power supply(1) through separate external pull resistors to ensure the inputs associated with these balls are held to a valid logic-high level, if unused. |
| R22 R23 R26 T27 T25 T24 T21 T22 U27 U26 V27 V25 V26 V24 V22 V23 |
GPMC0_AD0 GPMC0_AD1 GPMC0_AD2 GPMC0_AD3 GPMC0_AD4 GPMC0_AD5 GPMC0_AD6 GPMC0_AD7 GPMC0_AD8 GPMC0_AD9 GPMC0_AD10 GPMC0_AD11 GPMC0_AD12 GPMC0_AD13 GPMC0_AD14 GPMC0_AD15 |
Each of these balls must be connected to the corresponding power supply(1) or VSS through separate external pull resistors to ensure the inputs associated with these balls are held to a valid logic-high or logic-low level as appropriate to select the desired device boot mode. |
| AB1 D1 L7 L8 N7 N8 T7 T8 |
VDDS_DDR VDDS_DDR VDDS_DDR VDDS_DDR VDDS_DDR VDDS_DDR VDDS_DDR VDDS_DDR VDDS_DDR_C |
If DDRSS is not used, each of these balls must be connected directly to VSS. |
| E1 H1 T1 W1 M4 M3 L4 L6 M5 L3 N2 L2 R6 P1 N1 P2 P6 P4 P3 G2 H6 U4 AA2 D6 D2 F6 D3 G4 E2 G6 F3 H5 H2 K2 L1 J6 J4 J2 H3 V3 R2 R5 T2 R3 U2 U5 V2 Y2 W4 V5 W2 V6 W3 AA3 AA5 U6 |
DDR0_DQS0 DDR0_DQS1 DDR0_DQS2 DDR0_DQS3 DDR0_CAS_n DDR0_RAS_n DDR0_A0 DDR0_A1 DDR0_A2 DDR0_A3 DDR0_A4 DDR0_A5 DDR0_CAL0 DDR0_CK0 DDR0_CK0_n DDR0_CKE0 DDR0_CKE1 DDR0_CS0_n DDR0_CS1_n DDR0_DM0 DDR0_DM1 DDR0_DM2 DDR0_DM3 DDR0_DQ0 DDR0_DQ1 DDR0_DQ2 DDR0_DQ3 DDR0_DQ4 DDR0_DQ5 DDR0_DQ6 DDR0_DQ7 DDR0_DQ8 DDR0_DQ9 DDR0_DQ10 DDR0_DQ11 DDR0_DQ12 DDR0_DQ13 DDR0_DQ14 DDR0_DQ15 DDR0_DQ16 DDR0_DQ17 DDR0_DQ18 DDR0_DQ19 DDR0_DQ20 DDR0_DQ21 DDR0_DQ22 DDR0_DQ23 DDR0_DQ24 DDR0_DQ25 DDR0_DQ26 DDR0_DQ27 DDR0_DQ28 DDR0_DQ29 DDR0_DQ30 DDR0_DQ31 DDR0_RESET0_n |
If DDRSS is not used, leave unconnected.Note: The DDR0 pins in this list can only be left unconnected when VDDS_DDR and VDDS_DDR_C are connected to VSS. The DDR0 pins must be connected as defined in the DDR Board Design and Layout Guidelines, when VDDS_DDR and VDDS_DDR_C are connected to a power source. |
| Y9 | VDDS_MMC0 | If MMC0 is not used, each of these balls must be connected to any 1.8V power source that does not violate device power supply sequencing requirements. |
| E15 F14 AB8 AA10 AB14 AB15 AA16 AA8 E18 AB5 AA6 W7 E17 D17 F18 |
SERDES0_REXT SERDES1_REXT CSI0_RXRCALIB CSI1_RXRCALIB CSI2_RXRCALIB CSI3_RXRCALIB DSI0_TXRCALIB USB0_RCALIB USB1_RCALIB USB0_DM USB0_DP USB0_VBUS USB1_DM USB1_DP USB1_VBUS |
Each of these balls must be connected to VSS through an appropriate external pull resistor to ensure these balls are held to a valid logic-low level, if unused. Refer to Signal Descriptions footnote for appropriate value of pull resistor for each signal. |
| G9 AC1 AE1 AE2 AD1 AD3 AD2 AB4 AC2 AC3 AB3 AF1 AB2 |
VPP MMC0_CALPAD MMC0_CLK MMC0_CMD MMC0_DS MMC0_DAT0 MMC0_DAT1 MMC0_DAT2 MMC0_DAT3 MMC0_DAT4 MMC0_DAT5 MMC0_DAT6 MMC0_DAT7 |
Each of these balls must be left unconnected, if unused. |
| W15 Y15 W13 W16 Y13 |
VDDA_CORE_CSI_DSI VDDA_CORE_CSI_DSI VDDA_1P8_CSI_DSI VDDA_1P8_CSI_DSI VDDA_1P8_CSI_DSI |
If CSIRX0 and DSITX0 are not used and the device boundary scan function is required, each of these balls must be connected to valid power sources.If CSIRX0 and DSITX0 are not used and the device boundary scan function is not required, each of these balls can alternatively be connected directly to VSS. |
| AC7 AC6 AD6 AD5 |
CSI0_RXCLKN CSI0_RXCLKP CSI0_RXN0 CSI0_RXP0 |
If CSIRX0 is not used, leave unconnected. |
| AE5 AE4 |
CSI0_RXN1 CSI0_RXP1 |
If CSIRX0 is not used or only operated in 1-lane mode, leave unconnected. |
| AF4 AF3 |
CSI0_RXN2 CSI0_RXP2 |
If CSIRX0 is not used or only operated in 1-lane or 2-lane mode, leave unconnected. |
| AG3 AG2 |
CSI0_RXN3 CSI0_RXP3 |
If CSIRX0 is not used or only operated in 1-lane, 2-lane, or 3-lane mode, leave unconnected. |
| AE16 AE17 AD17 AD18 |
DSI0_TXCLKN DSI0_TXCLKP DSI0_TXN0 DSI0_TXP0 |
If DSITX0 is not used, leave unconnected. |
| AF15 AF16 |
DSI0_TXN1 DSI0_TXP1 |
If DSITX0 is not used or only operated in 1-lane mode, leave unconnected. |
| AG14 AG15 |
DSI0_TXN2 DSI0_TXP2 |
If DSITX0 is not used or only operated in 1-lane or 2-lane mode, leave unconnected. |
| AC18 AC19 |
DSI0_TXN3 DSI0_TXP3 |
If DSITX0 is not used or only operated in 1-lane, 2-lane, or 3-lane mode, leave unconnected. |
| AF23 AG24 AG22 AG23 AB20 AB21 AG20 AG21 AD21 AC21 AF19 AF18 AG17 AG18 AB19 AA20 AF21 AE20 AD20 AE19 |
OLDI0_A0N OLDI0_A0P OLDI0_A1N OLDI0_A1P OLDI0_A2N OLDI0_A2P OLDI0_A3N OLDI0_A3P OLDI0_A4N OLDI0_A4P OLDI0_A5N OLDI0_A5P OLDI0_A6N OLDI0_A6P OLDI0_A7N OLDI0_A7P OLDI0_CLK0N OLDI0_CLK0P OLDI0_CLK1N OLDI0_CLK1P |
If OLDI0 is not used, leave unconnected. |
| G7 J7 K7 A3 |
VMON_ER_VSYS VMON_1P8_SOC VMON_3P3_SOC WKUP_LFOSC0_XI |
Each of these balls must be connected to VSS through separate external pull resistors to ensure these balls are held to a valid logic-low level, if unused. |
All other unused signal balls with a Pad Configuration Register can be left unconnected with their multiplexing mode set to GPIO input and internal pull-down resistor enabled. Unused balls are defined as those which only connect to a PCB solder pad. This is the only use case where internal pull resistors are allowed as the only source/sink to hold a valid logic level. Any balls connected to a via, test point, or PCB trace are consider used and must not depend on the internal pull resistor to hold a valid logic level.
Internal pull resistors are weak and may not source enough current to maintain a valid logic level for some operating conditions. This can be the case when connected to components with leakage to the opposite logic level, or when external noise sources couple to signal traces attached to balls which are only pulled to a valid logic level by the internal resistor. Therefore, external pull resistors are recommended to hold a valid logic level on balls with external connections.
Many of the device IOs are turned off by default and external pull resistors may be required to hold inputs of any attached device in a valid logic state until software initializes the respective IOs. The state of configurable device IOs are defined in the BALL STATE DURING RESET RX/TX/PULL and BALL STATE AFTER RESET RX/TX/PULL columns of the Pin Attributes table. Any IO with its input buffer (RX) turned off is allowed to float without damaging the device. However, any IO with its input buffer (RX) turned on shall never be allowed to float to any potential between VILSS and VIHSS. The input buffer can enter a high-current state which could damage the IO cell if allowed to float between these levels.