SPRUI76B March   2017  – June 2022

 

  1.   Delfino TMS320F28379D controlCARD R1.3
  2.   Trademarks
  3. 1Introduction
  4. 2Errata
    1. 2.1 Warnings/Notes/Errata
    2. 2.2 Warnings About Specific controlCARD Revisions
  5. 3Getting Familiar With the controlCARD
    1. 3.1 F28379D controlCARD Features
    2. 3.2 Assumed Operating Conditions
    3. 3.3 Using the controlCARD
    4. 3.4 Experimentation Software
  6. 4Special Notes on Connectivity
    1. 4.1 xds100v2 Emulator and SCI/UART Connectivity
    2. 4.2 External Connector – J9
    3. 4.3 Evaluation of the Analog-to-Digital Converters (ADCs)
  7. 5Hardware References
  8. 6References
  9. 7Revision History

Introduction

As of January 2016, all kits based on the F28377D MCU will now be replaced with the new F28379D superset device. These two MCUs are identical except for the addition of the CLB on the F28379D MCU to enable Position Manager. If the CLB is not a requirement in your application, that feature can be left untouched and the MCU will perform like the F28377D.

Each controlCARD comes with a Hardware Developer’s Kit, a full set of files necessary to evaluate and develop with a C2000 device. These files include:

  • Schematics – Designed in Mentor PADS Logic
  • Bill of Materials (BOM)
  • Layout PCB files - Designed in Mentor layout
  • Gerber files

The Hardware Developer's Kit for the controlCARD can be found in the C2000Ware at the following location:

  • <install directory>\c2000\C2000Ware_x_xx_xx_xx\boards\controlCARDs\TMDSCNCD28379D\Rx_x
WARNING: When the controlCARD is used in a high-voltage setup, it is the user’s responsibility to confirm that the voltages and isolation requirements are identified and understood prior to energizing the board or simulation. When energized, the controlCARD or components connected to the controlCARD should not be touched. Furthermore, the capacitor A:C31 should be removed to minimize the possibility of leakage current flowing across the isolation barrier of the controlCARD.
Note:

This kit is designed to explore the functionality of the F2837x microcontrollers. Even though the controlCARD can be treated as a good reference design, it is not intended to be a complete customer design. Full compliance to safety, EMI/EMC, and other regulations are left to the designer of the final customer’s system.