SPRUIW8 November 2020
The F280025C boot ROM contains bootloading software that executes every time the device is powered on or reset. Two pins, GPIO24 and GPIO32, are wired to the Boot Select switch (S3). By default, both pins are set HIGH (1) so the device will boot from Flash. For more information on the F28002x boot modes, see the TMS320F28002x microcontrollers datasheet.
| BOOT MODE | GPIO24 (LEFT) | GPIO32 (RIGHT) |
|---|---|---|
| Boot from Parallel GPIO | 0 | 0 |
| Boot from SCI / Wait boot | 0 | 1 |
| Boot from CAN | 1 | 0 |
| Boot from Flash (default) | 1 | 1 |