SPRUJ15B November 2021 – October 2022
Figure 1-1 F2800137 controlCARDEach controlCARD comes with a Hardware Developer’s Kit, which is a full set of files necessary to evaluate and develop with a C2000 device. These files include:
The Hardware Developer's Kit for the controlCARD can be found in the C2000Ware at the following location:
<install directory>\c2000\C2000Ware_x_xx_xx_xx\boards\controlCARDs\TMDSCNCD2800137\Rx_x