SPRUJA7A November 2023 – April 2024
For the controlCARD to operate, the controlCARD MCU must be powered. This is done through the USB-C connector J3 on the controlCARD or by inputting 5 V through the HSEC connector using the accompanying baseboard. For example, if using a TMDSHSECDOCK docking station baseboard, 5 VDC can be input into the docking station J1 or J17. Then, S1 needs to be toggled to the appropriate position.
Based on the way the controlCARD is used, additional hardware settings are necessary (see Table 4-1).
MCU is not powered via type-C USB connector J2 on the controlCARD. This USB is to be used only for data-peripheral connection with the C2000 MCU.
| Switch | Debug using CCS IDE and the on-card XDS110 Emulator
(4-pin JTAG mode only) |
Debug using CCS IDE and an External Emulator using the Baseboard | Standalone (Boot from FLASH or other Boot Mode) |
|---|---|---|---|
| S4 | Position 1: ON (right, default) to connect the embedded XDS110 emulator to the MCU | Position 1: OFF (left) to disconnect the embedded XDS110 emulator from the MCU | Position 1: OFF (left) |
| Position 2: ON (right, default) to connect the embedded XDS110 UART COM port to the MCU GPIO28 pin. | Position 2: OFF (left) to disconnect the embedded XDS110 UART COM port to the MCU GPIO28 pin. | Position 2: OFF (left) | |
| J3 | Connect a USB-C cable between J3 and your computer | --- | --- |
|
In CCS, use this target configuration: TMS320F28P550SJ9 device with an XDS110 emulator, 4-pin JTAG mode only. |
|||
| S1 | Position 1 (GPIO24):
down- Logic 0 |
Position 1 (GPIO24):
down- Logic 0 |
Setup S3 as desired |
| Position 2 (GPIO32): up- Logic 1 |
Position 2 (GPIO32): up- Logic 1 |
||
| Putting the C2000 device into Wait Mode can reduce risk of connectivity issues | Putting the C2000 device into Wait Mode can reduce risk of connectivity issues | ||
| Baseboard JTAG connector (J2 on Docking Station) | --- | Connect an external emulator | --- |
Code Composer Studio is an Integrated
Development Environment (IDE) used to debug and develop software for the C2000
series of MCUs. CCS IDE can be downloaded from the following link:
http://www.ti.com/tool/ccstudio.
The following PDF documents are provided, as part of C2000Ware, to describe where each of the F28P55x MCU pins appears on the controlCARD connector/docking station:
More information on the controlCARD
docking station can be found in the C2000Ware at
the following location:
<install
directory>\c2000\C2000Ware_<rev>\boards\controlCARDs\TMDSCNCD28P55X\Rx_x.