SPRUJD3A July 2025 – October 2025 F28E120SB , F28E120SC
FILE: gpio_ex2_toggle.c
Configures the device GPIO through the sysconfig file. The GPIO pin is toggled in the infinite loop. In order to migrate the project within syscfg to any device, click the swtich button under the device view and select your
corresponding device to migrate, saving the project will auto-migrate your project settings.
: This example project has support for migration across our C2000 device families. If you are wanting to build this project from launchpad or controlCARD, please specify in the .syscfg file the board you're using. At any time you can select another device to migrate this example.