SPRUJD3A July 2025 – October 2025 F28E120SB , F28E120SC
eCAP modules can be synchronized with each other by selecting a common SYNCIN source. SYNCIN source for eCAP can be either software sync-in or external sync-in. The external sync-in signal can come from eCAP, X-Bar, or MCPWM. The SWSYNC of the eCAP module is logical ORed with the SYNC signal as shown in Figure 16-7. The SYNC signal is defined by the selection of ECAPxSYNCINSEL[SEL] as shown in Figure 16-8.
Figure 16-7 Details of the Counter and Synchronization Block