SPRUJD3A July 2025 – October 2025 F28E120SB , F28E120SC
To disable all interrupts, set the CPU global interrupt mask using DINT or SETC INTM. It is not necessary to add NOPs after setting INTM or modifying IER – the next instruction executes with interrupts disabled.
Individual interrupts can be disabled using the PIEIERx registers, but care must be taken to avoid race conditions. If an interrupt signal is already propagating when the PIEIER write completes, the signal can reach the CPU and trigger a spurious interrupt condition. To avoid this, use the following procedure:
Interrupt groups can be disabled using the CPU IER register. This cannot cause a race condition, so no special procedure is needed.
PIEIFR bits must never be cleared in software since the read/modify/write operation can cause incoming interrupts to be lost. The only safe way to clear a PIEIFR bit is to have the CPU take the interrupt. The following procedure can be used to bypass the normal ISR: