SPRUJH0B April 2025 – September 2025
To allow for more flexibility when evaluating the F28E12x MCU, this LaunchPad features multiple configurations for routing the GPIO35 and GPIO37 pins. By default, GPIO35 (RXD) and GPIO37 (TXD) are routed to the virtual COM port and are not available on the BoosterPack connector. These GPIO pins support both the SCIA peripheral and the high-speed UARTA peripheral. Alternatively, GPIO35 (TDI) and GPIO37 (TDO) can be routed as JTAG signals to the XDS110 debugger to enable debugging with 4-pin JTAG. When UART or 4-pin JTAG are not needed, the GPIOs can be routed to the BoosterPack connectors for BoosterPack standard functions.
The routing destination of these signal pairs are selected using the on-board switch S2, as described in Table 2-8.
| SEL1 (Left) | SEL2 (Right) | GPIO35 Function | GPIO37 Function | Intended Use Case |
|---|---|---|---|---|
| 0 | 0 | UART RXD | UART TXD | 2-pin cJTAG + serial UART |
| 0 | 1 | JTAG TDI | JTAG TDO | 4-pin JTAG |
| 1 | x | BP Header J1.3 | BP Header J1.4 | BoosterPack function |
Note that using 4-pin JTAG with serial UART communication to the virtual COM port is not supported on LAUNCHXL-F28E12X hardware. If UART communication is needed, use the 2-pin cJTAG + serial UART configuration.