SPRZ295Q April 2009 – January 2019 TMS320F28030 , TMS320F28030-Q1 , TMS320F28031 , TMS320F28031-Q1 , TMS320F28032 , TMS320F28032-Q1 , TMS320F28033 , TMS320F28033-Q1 , TMS320F28034 , TMS320F28034-Q1 , TMS320F28035 , TMS320F28035-EP , TMS320F28035-Q1
Figure 1 provides an example of the 2803x device markings and defines each of the markings. The device revision can be determined by the symbols marked on the top of the package as shown in Figure 1. Some prototype devices may have markings different from those illustrated. Figure 2 shows the device nomenclature.
Figure 1. Example of Device Markings | PACKAGE MARKING CODE | SILICON REVISION | REVISION ID
Address: 0x0883 |
COMMENTS |
|---|---|---|---|
| Blank | Indicates Revision 0 | 0x0000 | This silicon revision is available as TMX and TMS. |
| A | Indicates Revision A | 0x0001 | This silicon revision is available as TMS. |
Figure 2. Device Nomenclature