SPRZ342O January 2011 – April 2021 TMS320F28062 , TMS320F28062-Q1 , TMS320F28062F , TMS320F28062F-Q1 , TMS320F28063 , TMS320F28064 , TMS320F28065 , TMS320F28066 , TMS320F28066-Q1 , TMS320F28067 , TMS320F28067-Q1 , TMS320F28068F , TMS320F28068M , TMS320F28069 , TMS320F28069-Q1 , TMS320F28069F , TMS320F28069F-Q1 , TMS320F28069M , TMS320F28069M-Q1
Figure 2-1 provides an example of the 2806x package symbolization and defines each of the markings. The device revision can be determined by the symbols marked on the top of the package as shown in Figure 2-1. Some prototype devices may have markings different from those illustrated. Figure 2-2 shows an example of the device nomenclature.
Figure 2-1 Example
of Package Symbolization| SILICON REVISION CODE | SILICON REVISION | REVISION ID Address: 0x0883 |
COMMENTS |
|---|---|---|---|
| Blank (no second letter in prefix) |
Indicates Revision 0 | 0x0000 | This silicon revision is available as TMX. |
| A | Indicates Revision A | 0x0001 | This silicon revision is available as TMS. |
| B | Indicates Revision B | 0x0002 | This silicon revision is available as TMS. |