SPRZ362F November 2012 – October 2021 TMS320F28050 , TMS320F28051 , TMS320F28052 , TMS320F28052-Q1 , TMS320F28052F , TMS320F28052F-Q1 , TMS320F28052M , TMS320F28052M-Q1 , TMS320F28053 , TMS320F28054 , TMS320F28054-Q1 , TMS320F28054F , TMS320F28054F-Q1 , TMS320F28054M , TMS320F28054M-Q1 , TMS320F28055
Figure 2-1 provides an example of the 2805x package symbolization and defines each of the markings. The device revision can be determined by the symbols marked on the top of the package as shown in Figure 2-1. Some prototype devices may have markings different from those illustrated. Figure 2-2 shows an example of the device nomenclature.
Figure 2-1 Example of Package Symbolization| PACKAGE MARKING CODE | SILICON REVISION | REVISION
ID Address: 0x0883 |
COMMENTS |
|---|---|---|---|
| Blank | Indicates Revision 0(1) | 0x0000 | This silicon revision is available as TMX. |
| A | Indicates Revision A(1) | 0x0000 | This silicon revision is available as TMS. |
Figure 2-2 Device Nomenclature