SPRZ439I January 2017 – August 2026 TMS320F280040-Q1 , TMS320F280040C-Q1 , TMS320F280041 , TMS320F280041-Q1 , TMS320F280041C , TMS320F280041C-Q1 , TMS320F280045 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280049 , TMS320F280049-Q1 , TMS320F280049C , TMS320F280049C-Q1
Analog Subsystem: Software Configuration for Shared Reference Pins
0, A
Smaller pin-count packages of the F28004x device family have combined VREFHI pins. Software configuration bits are provided in the ANAREFPP register to disable all but one of the ganged references. This allows correct operation of internal reference mode in these circumstances. On production (TMS) devices, the Boot ROM will write these bits, and no further action will be required from the user. However, on some TMX devices, this write will not occur.
For TMX devices, the user should do the following writes one time before trying to configure the references for internal reference mode: