SPRZ439I January 2017 – August 2026 TMS320F280040-Q1 , TMS320F280040C-Q1 , TMS320F280041 , TMS320F280041-Q1 , TMS320F280041C , TMS320F280041C-Q1 , TMS320F280045 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280049 , TMS320F280049-Q1 , TMS320F280049C , TMS320F280049C-Q1
GPIO: Parasitic Path to VSS When Maximum VIH is Exceeded in Input Mode
A
If a voltage greater than maximum VIH (VDDIO + 0.3 V) is applied to the GPIO pins listed below, an internal parasitic path from the pin to VSS may be turned on. This parasitic current can impact the functional operation of the pin. This is more likely to occur at high temperature. The parasitic path will be removed when the IO is driven below VIL. The path will not reactivate until another overvoltage event occurs.
Pins configured for output-only mode (with no other drivers on the pin) will not see an overvoltage condition at the pin and are not affected by this advisory.
Pins configured in input or bidirectional mode can see an overvoltage condition in three primary ways:
If any of the above conditions apply for an input or bidirectional pin, insert a series resistor between the signal and the input pin. The series resistor should be placed close to the input pin.
If the overvoltage is due to overshoot (situations #1 or #2 above), a series resistor of 100 Ω or greater should be used.
If the overvoltage might be sustained (situation #3 above), a series resistor of 220 Ω or greater should be used.