SPRZ439I January 2017 – August 2026 TMS320F280040-Q1 , TMS320F280040C-Q1 , TMS320F280041 , TMS320F280041-Q1 , TMS320F280041C , TMS320F280041C-Q1 , TMS320F280045 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280049 , TMS320F280049-Q1 , TMS320F280049C , TMS320F280049C-Q1
LIN: Inconsistent Sync Field Error (ISFE) Flag/Interrupt Not Set When Sync Field is Erroneous
0, A, B, D
During LIN communications, if the Sync field received (on RX) is erroneous (that is, if the Sync field receives any value other than 0x55), the LIN does not set the ISFE Flag in the SCIFLR.ISFE register or trigger the ISFE interrupt. Communication gets terminated without data being received or the RX receive interrupt being set. There is no way for an application to detect an error in the Sync field. The application can detect if the Sync field is completely blank or if the Sync field is not received within the given tolerances (as explained in the TMS320F28004x Real-Time Microcontrollers Technical Reference Manual), but the application cannot detect any error in the value of Sync field.
Method 1: Keep polling the SCIFLR.RXRDY flag and time out if it is not set within a certain amount of time.
Use the following steps as a guideline:
Method 2: Configure the CPU timer to interrupt if the RX interrupt is not triggered. This method does not use CPU bandwidth.
Use the following steps as a guideline: