SPRZ439I January   2017  – August 2026 TMS320F280040-Q1 , TMS320F280040C-Q1 , TMS320F280041 , TMS320F280041-Q1 , TMS320F280041C , TMS320F280041C-Q1 , TMS320F280045 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280049 , TMS320F280049-Q1 , TMS320F280049C , TMS320F280049C-Q1

 

  1.   1
  2.   TMS320F28004x Real-Time MCUs Silicon Errata (Silicon Revisions D, B, A, 0)
  3. 1Usage Notes and Advisories Matrices
    1. 1.1 Usage Notes Matrix
    2. 1.2 Advisories Matrix
  4. 2Nomenclature, Package Symbolization, and Revision Identification
    1. 2.1 Device and Development Support Tool Nomenclature
    2. 2.2 Devices Supported
    3. 2.3 Package Symbolization and Revision Identification
  5. 3Silicon Revision D Usage Notes and Advisories
    1. 3.1 Silicon Revision D Usage Notes
      1. 3.1.1 PIE: Spurious Nested Interrupt After Back-to-Back PIEACK Write and Manual CPU Interrupt Mask Clear
      2. 3.1.2 FPU32 and VCU Back-to-Back Memory Accesses
      3. 3.1.3 Caution While Using Nested Interrupts
      4. 3.1.4 Security: The primary layer of defense is securing the boundary of the chip, which begins with enabling JTAGLOCK and Zero-pin Boot to Flash feature
    2. 3.2 Silicon Revision D Advisories
      1.      Advisory
      2.      Advisory
      3.      Advisory
      4.      Advisory
      5.      Advisory
      6.      Advisory
      7.      Advisory
      8.      Advisory
      9.      Advisory
      10.      Advisory
      11.      Advisory
      12.      Advisory
      13.      Advisory
      14.      Advisory
      15.      Advisory
      16.      Advisory
      17.      Advisory
      18. 3.2.1 Advisory
      19.      Advisory
      20.      Advisory
      21.      Advisory
      22.      Advisory
      23.      Advisory
      24. 3.2.2 Advisory
      25.      Advisory
      26.      Advisory
      27.      Advisory
      28.      Advisory
      29.      Advisory
      30. 3.2.3 Advisory
      31.      Advisory
      32.      Advisory
      33.      Advisory
      34. 3.2.4 Advisory
      35.      Advisory
  6. 4Silicon Revision B Usage Notes and Advisories
    1. 4.1 Silicon Revision B Usage Notes
    2. 4.2 Silicon Revision B Advisories
  7. 5Silicon Revision A Usage Notes and Advisories
    1. 5.1 Silicon Revision A Usage Notes
    2. 5.2 Silicon Revision A Advisories
      1.      Advisory
      2.      Advisory
      3.      Advisory
      4.      Advisory
      5.      Advisory
      6.      Advisory
  8. 6Silicon Revision 0 Usage Notes and Advisories
    1. 6.1 Silicon Revision 0 Usage Notes
    2. 6.2 Silicon Revision 0 Advisories
      1.      Advisory
      2.      Advisory
      3.      Advisory
  9. 7Documentation Support
  10. 8Trademarks
  11. 9Revision History

Advisory

GPIO: Signal Latch-up to VSS

Revision Affected

0

Details

The ESD structures on the pins listed below can be unintentionally turned on during functional operation, which will pull the pins to VSS. There will be approximately 40 mA of additional current on the VDDIO supply for each output pin in this condition.

  • GPIO16
  • GPIO17
  • GPIO24
  • GPIO25
  • GPIO26
  • GPIO27
  • GPIO35 (TDI)
  • GPIO37 (TDO)
  • GPIO40
  • GPIO41
  • GPIO42
  • GPIO43

The condition has not been observed below 70°C under normal operation. This condition can occur in input or output mode and with any of the mux functions. Designs with lightly loaded pins and fast switching signals are more likely to see the condition. Pins not bonded out in smaller pin-count packages can also enter the latch-up condition if they are toggled.

The latch-up condition can be ended by toggling the IO at a lower temperature.

Workarounds

Four workaround options are:

  1. Avoid using these pins on the revision affected.
  2. Avoid high-temperature operations on the revision affected.
  3. If the pin is configured as an input or output:

    Place a capacitor of 300 pF or greater between each of these pins and ground, placed as closely as possible to the device. This will slow down the fast signal and avoid triggering the condition. Larger capacitors will be more effective at filtering the transient but must be balanced against the system-level timing requirements of these pins.

    For input pins, a smaller capacitor may be possible when used in combination with option 4.

  4. If the pin is configured as an input:

    Connect a resistor in series with any other components on the board such that the total resistance of the driver plus the resistor is 1 kΩ or greater. The goal is to eliminate fast voltage transient seen at the pin. This will also limit the DC current if the ESD structure is activated due to noise.