SPRZ455G December 2020 – June 2026 DRA829J , DRA829J-Q1 , DRA829V , DRA829V-Q1 , TDA4VM , TDA4VM-Q1
USB: Race Condition while Reading TRB from System Memory in Device Mode
The following sequence will ensure that stale data is not transferred:
USB device controller uses 12-byte Transfer Request Block (TRB) data structures that are used to form a transfer ring in system memory. TRB contains the pointer to data buffer in memory that contains data to be transferred over USB or the location to store the data received over USB. Transfer ring management uses producer-consumer model where the software is the producer and Controller is the consumer. Ownership of a TRB is transferred between software and hardware using ‘Cycle’ bit field within the TRB. Software write of TRB into memory and hardware read of TRB from memory are expected to be atomic operations.
The issue arises because controller reads the TRB from system memory using two independent DMA transactions (8-byte transaction followed by a 4-byte transaction). As a result, TRB read operation by the controller is not atomic. If the software write to TRB occurs after hardware has read the first 8 bytes, this could lead to stale data transfer on IN transaction and stale data provided to software on OUT transaction.
The ‘Cycle’ bit is the least significant bit, which is read by the Controller in the second DMA transfer. Race condition exists because software write could be interleaved between the two read transactions. The following order of events could lead to corrupted data transfer on the USB bus:
This issue only affects Device mode.