SPRZ455G December 2020 – June 2026 DRA829J , DRA829J-Q1 , DRA829V , DRA829V-Q1 , TDA4VM , TDA4VM-Q1
Recommended POST selection via MCU_BOOTMODE[09:08]
The MCU_BOOTMODE[09:08] pins can be used to configure the Power-on-Selftest (POST) mode of operation. The effect of the MCU_BOOTMODE[09:08] depends on the TI factory setting for internal efuse override control. The options defined in the TRM are:

The recommended MCU_BOOTMODE[09:08] settings depends on the Device Type, as summarized in the Workaround section.
The Device Type is identified by the part number Y/Device Type designator, which is described in the SoC Data Manual chapter 10. This is illustrated in the following diagram:

For Device Type = C, 5, D
For Device Type = G, 0