SPRZ570C November   2023  – July 2025 AM263P2-Q1 , AM263P4 , AM263P4-Q1

 

  1.   1
  2.   Abstract
  3. 1Usage Notes and Advisories Matrices
  4. 2Silicon Revision 1.0 Usage Notes and Advisories
    1. 2.1 Silicon Revision 1.0 Usage Notes
      1.      i2324
      2.      i2488
    2. 2.2 Silicon Revision 1.0 Advisories
      1.      i2189
      2.      i2310
      3.      i2374
      4.      i2311
      5.      i2345
      6.      i2351
      7.      i2352
      8.      i2353
      9.      i2354
      10.      i2356
      11.      i2357
      12.      i2358
      13.      i2359
      14.      i2383
      15.      i2392
      16.      i2393
      17.      i2394
      18.      i2401
      19.      i2404
      20.      i2405
      21.      i2426
      22.      i2427
      23.      i2428
      24.      i2433
      25.      i2438
      26.      i2439
      27.      i2485
      28.      i2486
  5. 3Trademarks
  6. 4Revision History

i2310

USART: Erroneous clear/trigger of timeout interrupt

Details:

The USART may erroneously clear or trigger the timeout interrupt when RHR/MSR/LSR registers are read.

Workaround(s):

For CPU use-case.

  • If the timeout interrupt is erroneously cleared:
    • This is Valid since the pending data inside the FIFO will retrigger the timeout interrupt
  • If timeout interrupt is erroneously set, and the FIFO is empty, use the following SW workaround to clear the interrupt:
    • Set a high value of timeout counter in TIMEOUTH and TIMEOUTL registers
    • Set EFR2 bit 6 to 1 to change timeout mode to periodic
    • Read the IIR register to clear the interrupt
    • Set EFR2 bit 6 back to 0 to change timeout mode back to the original mode

For DMA use-case.

  • If timeout interrupt is erroneously cleared:
    • This is valid since the next periodic event will retrigger the timeout interrupt
    • User must ensure that RX timeout behavior is in periodic mode by setting EFR2 bit6 to 1
  • If timeout interrupt is erroneously set:
    • This will cause DMA to be torn down by the SW driver
    • Valid since next incoming data will cause SW to setup DMA again