SPRZ582B March 2025 – October 2025 AM62L
MMCSD: HS200 write failures
The MMC0 interface has the potential for write failures when issuing multiple block writes operating in HS200 mode with excessive IO supply noise.
To minimize IO supply noise follow below best practices and refer to the linked application note:
Implement a software recovery mechanism that re-issues the failed multiple block write with minimum 5μs delay between blocks to reduce noise. One way to achieve this delay is using single block writes for the failed multiple block write.