SPRZ582B March   2025  – October 2025 AM62L

 

  1.   1
  2. 1Usage Notes and Advisories Matrices
    1. 1.1 Devices Supported
  3. 2Silicon Usage Notes and Advisories
    1. 2.1 Silicon Usage Notes
      1.      i2330
      2.      i2351
    2. 2.2 Silicon Advisories
      1.      i2189
      2.      i2208
      3.      i2249
      4.      i2253
      5.      i2278
      6.      i2279
      7.      i2310
      8.      i2311
      9.      i2312
      10.      i2493
      11.      i2383
      12.      i2401
      13.      i2409
      14.      i2431
      15.      i2435
      16.      i2461
      17.      i2462
      18.      i2463
      19.      i2464
      20.      i2465
      21.      i2466
      22.      i2467
      23.      i2469
      24.      i2470
      25.      i2471
      26.      i2473
      27.      i2474
      28.      i2160
      29.      i2481
      30.      i2482
      31.      i2484
      32.      i2487
  4.   Trademarks
  5. 3Revision History

i2471

Boot: Certain primary/backup boot mode combinations fail

Details:

Certain primary/backup boot order combinations will fail dual stage boot in the backup boot mode

If primary boot has an offset based start point (eg, O/Q/SPI, Serial NAND, GPMC NAND, eMMC boot)

and backup boot mode is filesystem based (eg, SD card, eMMC with UDA, USB MSC), then boot will fail in the backup boot mode (during second stage processing), if primary boot is not successful

OR

If primary boot is filesystem based (eg, SD card, eMMC with UDA, USB MSC),

and backup boot mode has an offset based start point (eg, O/Q/SPI, Serial NAND, GPMC NAND, eMMC boot), then boot will fail in the backup boot mode (during second stage processing), if primary boot is not successful

Workaround(s):

None. Do not select the affected boot combinations.