SPVA062 June   2026 PCM4220 , PCM4222 , TLV320ADC6120 , TLV320ADC6140

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2Detailed Description
    1. 2.1 Why Idle Tones?
    2. 2.2 How To Improve Idle Channel Spectrum in Audio Band
      1. 2.2.1 Example 1 – TLV320ADC6120
      2. 2.2.2 Example 2 – PCM4222
  6. 3Summary
  7. 4References

Why Idle Tones?

Figure 2-1 presents simple first-order Δ-Σ modulator with a one-bit output. The output of the integrator is digitized through a comparator (or a one-bit ADC). This output is fed back to the input signal through a one-bit DAC. This error signal is the input to the integrator.

 Delta-Sigma ModulatorFigure 2-1 Delta-Sigma Modulator

This conversion is done at a rate much higher than the overall sampling rate of the ADC itself. This helps with:

  1. Relaxed anti-aliasing filter bandwidth requirements, since the filter's bandwidth can be higher than the Nyquist bandwidth of the ADC.
  2. Lower noise due to averaging/decimation of the comparator output down to the ADC's sampling rate.

At near-idle inputs (0V), the output of the comparator stage has a repeating pattern of 0101…, which translates to a spike at F m o d 2 , Fmod being the sampling frequency of the modulator. With non-idealities like

  1. Offset in the input path due to mismatches
  2. Fmod causing modulation of the voltage reference

The spike frequencies change to F m o d ± Δ f 2 , the Δf is the frequency change brought about by these non-idealities. These spikes, when decimated to an output sampling rate of Fs, can result in the "idle tones" being observed in the audible band of the ADC.

While the integrated noise can still be low and within spec, having tones above the actual noise floor is still an undesirable artifact in applications where the output is amplified before post-processing or passed to a speaker amplifier. While modern day audio ADCs are designed with multi-bit Δ-Σ modulators to obtain improved noise performance, repeating patterns with idle inputs still result in tones in the audio spectrum.

However, these repeating patterns are not there when the input is a moving signal. Figure 2-2 shows the FFT spectrum on the TLV320ADC6120 ADC (a) when the inputs are idle, and (b) with a -60dBFS, 1kHz sinusoidal signal. Figure 2-3 shows the FFT spectrums under the same input conditions on the PCM4222 ADC.

As is clearly visible in both Figure 2-2 and Figure 2-3, these tones disappear with input signals moving at amplitudes as low as -60dBFS.

 FFT Spectrum for TLV320ADC6120Figure 2-2 FFT Spectrum for TLV320ADC6120
 FFT Spectrum of PCM4222Figure 2-3 FFT Spectrum of PCM4222