SSZTDE7 October 2026 TAS2573 , TAS2781
If a low-frequency bass transient (such as a snare drum hit or an explosion in a movie) threatens to push the cone past its Xmax, the excursion protection algorithm deploys rapid, targeted countermeasures. A brief digital delay buffer (typically a few milliseconds) enables the DSP to see a dangerous peak before it actually reaches the amplifier stage, giving the algorithm time to apply a precise, instantaneous peak attenuation to that specific waveform cycle. See Figure 8.
In Figure 9, the blue curve represents the smart amplifier’s estimated excursion, while the red lines indicate the Xmax limits. The amplifier dynamically modulates the audio to ensure that the speaker is always within reliable excursion limits.