STDA010 January 2026 LM25180-Q1 , LM5155-Q1 , SN6507-Q1 , UCC14240-Q1 , UCC34141-Q1
Single-stage topology is currently emerging as the preferred choice for onboard chargers (OBCs) in electric vehicles (EVs) by demonstrating a higher power density, a smaller size, and potentially lower costs when compared to traditional, dual-stage OBCs with PFC (power factor correction) and DC-DC converter stages. The matrix converter is generally the most popular topology for single-stage OBCs. In the OBCs design, the isolated bias power supply contains a major part of the circuit, which is primarily used to supply the required power to the gate drivers. This paper proposes architectures that offer efficient, isolated bias power supplies especially focused on single-stage OBCs. There are several architectures available to gate drivers in a single-stage onboard charger which incorporate an isolated bias power supply. These architectures also directly influence the choice of topologies, and related devices used, for the isolated bias power supply in the single-stage onboard charger.