As part of the SimpleLink™ Academy TI provides training material for the Wi-SUN® FAN implementation including hands-on examples using
the CC13x2R7 and CC13x4R10 LaunchPads. The examples are split into three parts:
- Fundamentals to Wi-SUN® FAN:
This training guides the user on how to create a simple Wi-SUN® FAN using one
border router connected to a host PC running PySpinel CLI to control the
network. Basic serial commands to start the network and ping connected nodes are
explained.
- Over-the-Air Download: This training explains the
concept of OAD using Wi-SUN®, the memory
layout necessary for saving multiple images and how to setup the OAD environment
and perform the download.
- CoAP Messaging: This training is intended to
introduce fully embedded router nodes to transmit CoAP messages between the BR
and RN. Examples are given for confirmable and non-confirmable CoAP messages. An
example for an EV charger application sending status information to the BR is
given.
Find these trainings through the links
above or on dev.ti.com.