SWRA770 august   2023 CC2564C

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Demo Overview
  5. 2Running the Bluetooth Code
  6. 3Demo Application
    1. 3.1 Device 1 (Host/HID Host) Setup on the Demo Application
    2. 3.2 Device 2 (Client/HID Device Setup on the Demo Application
    3. 3.3 Initiating Connection from the HID Host
    4. 3.4 Initiating Connection from HID Device
    5. 3.5 Communication Between Host and Device
  7. 4Application Commands
  8. 5Gap Commands
    1. 5.1  Help (DisplayHelp)
    2. 5.2  Inquiry
    3. 5.3  Display Inquiry List
    4. 5.4  Pair
    5. 5.5  End Pairing
    6. 5.6  PIN Code Response
    7. 5.7  Pass Key Response
    8. 5.8  User Confirmation Response
    9. 5.9  Set Discoverability Mode
    10. 5.10 Set Connectability Mode
    11. 5.11 Set Pairability Mode
    12. 5.12 Change Simple Pairing Parameters
    13. 5.13 Get Local Address
    14. 5.14 Set Local Name
    15. 5.15 Get Local Name
    16. 5.16 Set Class of Device
    17. 5.17 Get Class of Device
    18. 5.18 Get Remote Name
  9. 6Human Interface Demo Profile
    1. 6.1 Host
      1. 6.1.1  Connect Remote HID Device
      2. 6.1.2  Close Connection
      3. 6.1.3  Control Request
      4. 6.1.4  Get Report Request
      5. 6.1.5  Set Report Request
      6. 6.1.6  Get Protocol Request
      7. 6.1.7  Set Protocol Request
      8. 6.1.8  Get Idle Request
      9. 6.1.9  Set Idle Request
      10. 6.1.10 Data Write
    2. 6.2 Client
      1. 6.2.1 Get Report Response
      2. 6.2.2 Set Report Response
      3. 6.2.3 Get Protocol Response
      4. 6.2.4 Set Protocol Response
      5. 6.2.5 Get Idle Response
      6. 6.2.6 Set Idle Response
  10. 7References
  11. 8Revision History

Set Protocol Response

Description

The following function is responsible for sending a response for an outstanding SET_PROTOCOL transaction to the remote HID Host. This function returns zero on successful execution and a negative value on all errors.

Parameters

SetProtocolResponse requires one parameter which is ResultType, 0= rtSuccessful, 1= rtNotReady, 2= rtErrInvalidReportID, 3= rtErrUnsupportedRequest, 4= rtErrInvalidParameter,5= rtErrUnknown, 6= rtErrFatal, 7= rtData.

Possible Return Values

  • (0) HID_Set_Protocol_Response: Function Successful
  • (-4) FUNCTION_ERROR
  • (-6) INVALID_PARAMETERS_ERROR
  • (-8) INVALID_STACK_ID_ERROR
  • (-103)BTPS_ERROR_FEATURE_NOT_AVAILABLE
  • (-1000)BTHID_ERROR_INVALID_PARAMETER
  • (-1001)BTHID_ERROR_NOT_INITIALIZED
  • (-1002)BTHID_ERROR_INVALID_BLUETOOTH_STACK_ID
  • (-1005)BTHID_ERROR_INVALID_OPERATION
  • (-1006)BTHID_ERROR_REQUEST_OUTSTANDING

API Call

HID_Set_Protocol_Response(BluetoothStackID, HIDID, (HID_Protocol_Type_t)TempParam->Params[0].intParam)

API Prototype

int BTPSAPI HID_Set_Protocol_Response(unsigned int BluetoothStackID, unsigned int HIDID, HID_Result_Type_t ResultType)

Description of API

The following function is responsible for sending the appropriate Response to an outstanding SET_PROTOCOL transaction. This function accepts the Bluetooth Stack ID of the Bluetooth Stack which is to send the response and the HID ID for which the connection has been established. The third parameter to this function is the Result Type that is to be associated with this response. The rtData Result Type is Invalid for use with this function. If the rtSuccessful through rtErrFatal Result Types are specified then this function responds to the SET_PROTOCOL Transaction with a HANDSHAKE response that has a Result Code parameter that matches the specified Result Type. This function returns zero if successful, or a negative return error code if there was an error.