SWRA770 august   2023 CC2564C

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Demo Overview
  5. 2Running the Bluetooth Code
  6. 3Demo Application
    1. 3.1 Device 1 (Host/HID Host) Setup on the Demo Application
    2. 3.2 Device 2 (Client/HID Device Setup on the Demo Application
    3. 3.3 Initiating Connection from the HID Host
    4. 3.4 Initiating Connection from HID Device
    5. 3.5 Communication Between Host and Device
  7. 4Application Commands
  8. 5Gap Commands
    1. 5.1  Help (DisplayHelp)
    2. 5.2  Inquiry
    3. 5.3  Display Inquiry List
    4. 5.4  Pair
    5. 5.5  End Pairing
    6. 5.6  PIN Code Response
    7. 5.7  Pass Key Response
    8. 5.8  User Confirmation Response
    9. 5.9  Set Discoverability Mode
    10. 5.10 Set Connectability Mode
    11. 5.11 Set Pairability Mode
    12. 5.12 Change Simple Pairing Parameters
    13. 5.13 Get Local Address
    14. 5.14 Set Local Name
    15. 5.15 Get Local Name
    16. 5.16 Set Class of Device
    17. 5.17 Get Class of Device
    18. 5.18 Get Remote Name
  9. 6Human Interface Demo Profile
    1. 6.1 Host
      1. 6.1.1  Connect Remote HID Device
      2. 6.1.2  Close Connection
      3. 6.1.3  Control Request
      4. 6.1.4  Get Report Request
      5. 6.1.5  Set Report Request
      6. 6.1.6  Get Protocol Request
      7. 6.1.7  Set Protocol Request
      8. 6.1.8  Get Idle Request
      9. 6.1.9  Set Idle Request
      10. 6.1.10 Data Write
    2. 6.2 Client
      1. 6.2.1 Get Report Response
      2. 6.2.2 Set Report Response
      3. 6.2.3 Get Protocol Response
      4. 6.2.4 Set Protocol Response
      5. 6.2.5 Get Idle Response
      6. 6.2.6 Set Idle Response
  10. 7References
  11. 8Revision History

Set Report Request

Description

The following function is responsible for sending a SET_REPORT Transaction to the remote HID Device. This function returns zero on successful execution and a negative value on all errors.

Parameters

SetReportRequest uses one parameter, ReportType 0 = rtOther, 1 = rtInput, 2 = rtOutput, 3 = rtFeature.

Possible Return Values

  • (0)HID_Set_Report_Request: Function Successful.
  • (-4) FUNCTION_ERROR
  • (-6)INVALID_PARAMETERS_ERROR
  • (-103)BTPS_ERROR_FEATURE_NOT_AVAILABLE
  • (-1000)BTHID_ERROR_INVALID_PARAMETER
  • (-1001)BTHID_ERROR_NOT_INITIALIZED
  • (-1002)BTHID_ERROR_INVALID_BLUETOOTH_STACK_ID
  • (-1005)BTHID_ERROR_INVALID_OPERATION
  • (-1006)BTHID_ERROR_REQUEST_OUTSTANDING

API Call

HID_Set_Report_Request(BluetoothStackID, HIDID, (HID_Report_Type_Type_t)TempParam->Params[1].intParam, size of(GenericMouseReport), GenericMouseReport)

API Prototype

int BTPSAPI HID_Set_Report_Request(unsigned int BluetoothStackID, unsigned int HIDID, HID_Report_Type_Type_t ReportType, Word_t ReportPayloadSize, Byte_t*ReportDataPayload)

Description of API

The following function is responsible for sending a SET_REPORT request to the remote device. This function accepts as input the Bluetooth Stack ID of the Bluetooth Stack which is to send the transaction and the HID ID for which the connection has been established. The third parameter is the type of report being sent. Note that rtOther is an Invalid Report Type for use with this function. The final two parameters to this function are the length of the Report Payload to send and a pointer to the Report Payload that is sent. This function returns zero if successful or a negative return error code if there was an error.

Note: Control Channel transfers have two phases, a Request by the host and a Response by the device. Only ONE host control channel Request can be outstanding at a time. Reception of an HID Set Report Confirmation event indicates that a Response has been received and the Control Channel is now free for further transactions.