SWRA834A May   2025  – February 2026 CC2340R5 , CC2340R5-Q1 , CC2744R7-Q1 , CC2745P10-Q1 , CC2745R10-Q1 , CC2745R7-Q1 , CC2755R10

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1 Introduction
  5. 2 Reference Designs
    1. 2.1 LP-EM-CC2340R53
    2. 2.2 LP-EM-CC2340R5
    3. 2.3 LP-EM-CC2340R5-Q1
    4. 2.4 LP-EM-CC2340R5-RGE-4x4-IS24
    5. 2.5 LP-EM-CC2745R10-Q1
  6. 3 Schematic
    1. 3.1 Schematic Overview
      1. 3.1.1 48MHz Crystal
      2. 3.1.2 32.768kHz Crystal
      3. 3.1.3 Filter
      4. 3.1.4 Decoupling Capacitors
      5. 3.1.5 Antenna Components
      6. 3.1.6 RF Shield
    2. 3.2 I/O Pins Drive Strength
    3. 3.3 Bootloader Pins
    4. 3.4 Serial Wire Debug (SWD) Pins
  7. 4 PCB Layout
    1. 4.1 Board Stack-Up
    2. 4.2 LC Filter
    3. 4.3 Decoupling Capacitors
    4. 4.4 Placement of Crystal Load Capacitors
    5. 4.5 Current Return Path
    6. 4.6 DC/DC Regulator
    7. 4.7 Antenna Matching Components
    8. 4.8 Transmission Lines
    9. 4.9 Electromagnetic Simulation
  8. 5 Antenna
  9. 6 Crystal Tuning
    1. 6.1 CC23xx and CC27xx Crystal Oscillators
    2. 6.2 Crystal Selection
    3. 6.3 Tuning the LF Crystal Oscillator
    4. 6.4 Tuning the HF Crystal Oscillator
  10. 7 Optimum Load Impedance
  11. 8 PA Table
  12. 9 Power Supply Configuration
    1. 9.1 Introduction to Power Supply
    2. 9.2 DC/DC Converter Mode
    3. 9.3 Global LDO Mode
  13. 10Board Bring-Up
    1. 10.1 Power On
    2. 10.2 RF Test: SmartRF Studio
    3. 10.3 RF Test: Conducted Measurements
      1. 10.3.1 Sensitivity
      2. 10.3.2 Output Power
    4. 10.4 Hardware Troubleshooting
      1. 10.4.1 No Link: RF Settings
      2. 10.4.2 No Link: Frequency Offset
      3. 10.4.3 Poor Link: Antenna
      4. 10.4.4 Bluetooth Low Energy: Device Does Advertising But Cannot Connect
      5. 10.4.5 Poor Sensitivity: Background Noise
      6. 10.4.6 High Sleep Power Consumption
  14. 11Summary
  15. 12References
  16. 13Revision History

Output Power

  1. Disconnect the antenna and perform conducted measurements at the SMA connector or solder a semi-rigid coax cable at the 50Ω point.
  2. Preferred method: use a spectrum analyzer (SA). Use 2MHz RBW for measuring output power.
  3. If an SA is not available, then use a LaunchPad with a SMA connection point. Use coaxial cables and attenuation between the LaunchPad SMA connector and the 50Ω point on the custom board. Use SmartRF Studio and set the Launchpad in Continuous RX and read the RSSI. Note, that the RSSI has a given tolerance so the measurement is not as accurate as the preferred method.

For more guidance on RF testing, refer to Basic RF Testing of CCxxxx Devices.