SWRU439M October   2015  – April 2022

 

  1.   Trademarks
  2. 1Introduction
  3. 2Overview
    1. 2.1 Sensor Controller and AUX Domain Hardware Overview
      1. 2.1.1 Hardware Functionality
      2. 2.1.2 Power and Clock Management
        1. 2.1.2.1 CC13x0 and CC26x0 Operation Modes
        2. 2.1.2.2 CC13x2 and CC26x2 Operation Modes
        3. 2.1.2.3 Communication With the System CPU Application
    2. 2.2 Sensor Controller Interface Driver
      1. 2.2.1 Tailored How-To-Use Guide
      2. 2.2.2 Doxygen Documentation
    3. 2.3 Sensor Controller Programming Model
    4. 2.4 Sensor Controller Tasks
      1. 2.4.1 Data Structures
      2. 2.4.2 Task Code Blocks
      3. 2.4.3 High-Level Program Flow
    5. 2.5 Task Testing and Debugging
    6. 2.6 Run-Time Logging
  4. 3Prerequisites
    1. 3.1 Driver
    2. 3.2 Examples
  5. 4Installation
    1. 4.1 Sensor Controller Studio for Windows
      1. 4.1.1 Update Service
    2. 4.2 Sensor Controller Studio CLI for Linux (64-Bit)
  6. 5Sensor Controller Studio Tutorials
  7. 6Sensor Controller Studio Walkthrough
    1. 6.1  Start Page and Navigation
    2. 6.2  Documentation
    3. 6.3  Open the Example
    4. 6.4  Project Panel
    5. 6.5  Task Panel Settings
    6. 6.6  Constants and Data Structures Panel
    7. 6.7  Task Code Editor Panels
    8. 6.8  I/O Mapping Panel
    9. 6.9  Code Generator Panel
    10. 6.10 Compiling Example Applications in IAR or CCS
    11. 6.11 Task Testing Panel
      1. 6.11.1 Task Testing Setup
      2. 6.11.2 Task Testing Session
      3. 6.11.3 Data Handling
      4. 6.11.4 Task Debugging Panel
    12. 6.12 Run-Time Logging Panel
      1. 6.12.1 Run-Time Logging Setup
      2. 6.12.2 Run-Time Logging Session
  8. 7References
  9. 8Revision History

Project Panel

The project panel contains settings that apply to the entire project, and allows for tasks to be added and removed (see Figure 6-4).

GUID-5C1E75A1-59B3-4C17-A523-3683CE24D567-low.png Figure 6-4 Project Settings Panel

The project settings include:

  • Project name and description: These are included in the generated SCIF driver setup header file.
  • Operating system: Select the operating system that affects which SCIF OSAL files are output.
  • Source code prefix (optional): If needed, specify a prefix that will be added to relevant parts of the driver setup (including file names). This allows for multiple SCIF driver setups in one application.
  • Source code output directory: Specify the path of the generated output by the absolute path or path relative to the Sensor Controller project file (*.scp).
  • Target chip: Select the target chip by specifying name, revision, and package. These settings affect which task resources are available, I/O mapping, task testing, and runtime logging.

Sensor Controller tasks can be added to and removed from the project in the bottom section.

It is possible to have multiple projects open at the same time.

Note:

The Save project and Close project commands apply only to the currently selected project in the project tree.