SWRU548C February 2019 – September 2021 CC3235MODAS , CC3235MODASF , CC3235MODS , CC3235MODSF
Table 2-7 lists the push-button definitions.
| Reference | Use | Comments |
|---|---|---|
| SW1 | RESET | This is used to reset the CC3235MOD device. This signal is also output on the 20-pin connector to reset any external BoosterPack which may be stacked. The reset can be isolated using the RST jumper at the isolation block. |
| SW2 | GPIO_13 | When pushed, GPIO_13 is pulled to VCC. |
| SW3 | GPIO_22 | When pushed, GPIO_22 is pulled to VCC. |
| SW4 | Factory default | Pressing this button and toggling RESET restores the factory default image on the serial flash. This can be used to recover a corrupted serial flash, provided the s-flash was programmed with a recovery image. |
Table 2-8 lists the LED indicators.
| Reference | Color | Use | Comments |
|---|---|---|---|
| D1, D2 | Green and Red | Debug | Indicates the state of the JTAG emulator. For TI use only. |
| D3 | Yellow | nRESET | Indicates the state of the NRESET pin. If this LED is on, the device is functional. |
| D4 | Red | Power | Indicates when the 3.3-V power is supplied to the board. |
| D7 | RGB | GPIO_09 | Glows when the GPIO is logic-1. |
| RGB | GPIO_10(1) | Glows when the GPIO is logic-1. | |
| RGB | GPIO_11(1) | Glows when the GPIO is logic-1. | |
| D8 | Red | Factory Reset | Indicates that the push-button for the factory reset is pressed. |