SWRU548C February 2019 – September 2021 CC3235MODAS , CC3235MODASF , CC3235MODS , CC3235MODSF
The RF section of this wireless module gets top priority in terms of layout. It is very important for the RF section to be laid out correctly to ensure optimum performance from the module. A poor layout can cause low-output power, EVM degradation, sensitivity degradation, and mask violations.
Figure 3-5 shows the RF placement and routing of the CC3235MODSF module.
Figure 3-5 RF Section LayoutUse the following RF layout recommendations for the CC3235MODx module:
For optimal RF performance, ensure the copper cut out on the top layer under the RF-BG pin (pin 31) is as shown in Figure 3-6.
Figure 3-6 Top Layer Copper Pullback on RF Pads