SWRU587A November 2021 – March 2023 AWR2944 , IWR2944
This is a drop-down menu that prompts users to select the matching SDK version as the one running on the mmWave device. If the version does not match, then the GUI prompts an error when using the Send Config to mmWave Device button or Load config from PC and send button. However, there is no such check done when using the Save config to PC button, and users can choose the SDK version for which the compatible configuration should be generated.