SWRU629C September 2024 – April 2026
SimpleLink Wi-Fi toolbox is a GUI-based tool for the evaluation, programming, and testing of CC35xx designs during development and certification. Radio Tool is one of the tools included in the toolbox that allows for RF testing. The tool enables low-level radio testing capabilities by manually setting the radio into transmit or receive modes. Usage of the tool requires familiarity and knowledge of radio circuit theory and radio test methods. To perform conducted RF testing on the LP-EM-CC35X1, refer to Section 2.4. Note that a rework can be needed.
The user can download this tool from the CC35xx product page on ti.com.