SWRU629C September   2024  – April 2026

 

  1.   1
  2.   Description
  3.   Features
  4.   4
  5. 1Evaluation Module Overview
    1. 1.1 Introduction
    2. 1.2 Kit Contents
    3. 1.3 Specification
    4. 1.4 Device Information
  6. 2Hardware
    1. 2.1 Wired Connections, Jumper Settings, Buttons, and LEDs
      1. 2.1.1  SWD Interface
      2. 2.1.2  I2C Connections
        1. 2.1.2.1 Default I2C Addresses
      3. 2.1.3  UART Signals
      4. 2.1.4  SD Card Interface
      5. 2.1.5  External Memory Interface
      6. 2.1.6  ADC Interface
      7. 2.1.7  Reset Pullup Jumper
      8. 2.1.8  Push Buttons
      9. 2.1.9  LED Indicators
      10. 2.1.10 LaunchPad Header Pin Assignment
    2. 2.2 Power
      1. 2.2.1 VIO Selection
      2. 2.2.2 Measure the CC35xxE Current Draw
        1. 2.2.2.1 Low Current Measurement (LPDS)
        2. 2.2.2.2 Active Current Measurement
    3. 2.3 Clocking
    4. 2.4 Conducted RF Testing
    5. 2.5 Evaluation Setup
      1. 2.5.1 Wi-Fi Toolbox LP-EM-CC35X1 Hardware Setup
        1. 2.5.1.1 HW Prerequisites
  7. 3Hardware Design Files
    1. 3.1 Schematics
    2. 3.2 PCB Layouts
    3. 3.3 Bill of Materials (BOM)
  8. 4Additional Information
    1. 4.1 Trademarks
  9. 5Revision History

HW Prerequisites

  • Windows 10 64-bit or Ubuntu 18 (or higher) 64-bit operation system
  • Latest Chrome web browser
  • Installation of Simplelink Wi-Fi Toolbox
  • LP-EM-CC35X1
  • LP-XDS110 or LP-XDS110ET debugger for SWD communication

The LP-XDS110 enables direct communication to the CC35xx device via the SWD interface. This allows external tools, such as the Radio Tool, to send commands directly to the device without the use of flashing the application image.

Note:

When using Simplelink Wi-Fi Toolbox, the default flash populated on the board is IS25WJ064F. Users must choose the correct flash option when prompted by the GUI.

LP-EM-CC35X1, LP-EM-CC35X1ET Radio Tool Flash Selection
                        Example Figure 2-26 Radio Tool Flash Selection Example

LP-EM-CC35X1 supports a variety different flash options. The list of supported flashes can be found in the SDK release notes on CC3551E product page.

For LP-EM-CC35X1ET users only, it is also important that the correct PSRAM type is selected. Users must select Stacked 8MB AP Memory. Users not using LP-EM-CC35X1ET must select No PSRAM for this option.

LP-EM-CC35X1, LP-EM-CC35X1ET