SWRU640 March 2026
Figure 2-8 shows the Daisy Chain interface, also known as the Vertical Interface (VIF) portion of the EVM. This interface allows the user to connect multiple CSU boards in a daisy chain configuration via daisy chain cables also shown in Figure 2-8.
Figure 2-8 BQ Daisy Chain Interface and CableThe board designated to communicate wirelessly with the wireless main MCU in a WBMS network is considered the base device. This base device is responsible for collecting data from all stacked devices and transmitting the data wirelessly to the wireless main device. The wireless main device can then interface with a host MCU or PC to then transfer the data to the user via a Graphical User Interface (GUI) or through UART/SPI data packets.
To configure multiple boards in a daisy chain configuration, the user will connect the daisy chain cable between COMH of the base device and COML of the next device in the daisy chain, which will be considered stack 1 or “S1”. This COMH to COML connection configuration will continue down the daisy chain between S1 and S2, and so on.
Figure 2-9 BQ Isolation Circuitry for VIF CommunicationFigure 2-9 shows the isolation portion of the VIF communication interface. This section contains series and termination resistors, Transient Voltage Suppressor (TVS) diodes, and isolation capacitors to keep the device protected from any noise that may be induced onto the communication lines.