SWRZ062F September   2015  – December 2022 CC1310

 

  1.   CC1310 SimpleLink™ Ultra-Low-Power Sub-1 GHz Wireless MCU Silicon Revisions B, A
  2.   Trademarks
  3. 1Advisory Matrix
  4. 2Nomenclature, Package Symbolization, and Revision Identification
    1. 2.1 Device and Development Support-Tool Nomenclature
    2. 2.2 Devices Supported
    3. 2.3 Package Symbolization and Revision Identification
  5. 3Silicon Revision B Advisories
    1.     Advisory 02
    2.     Advisory 03
    3.     Advisory 04
    4.     Advisory 05
    5.     Advisory 06
    6.     Advisory 07
    7.     Advisory 08
    8.     Advisory 09
    9.     Advisory 10
    10.     Advisory 11
    11.     Advisory 12
    12.     Advisory 13
    13.     Advisory 14
    14.     Advisory 15
    15.     Advisory 16
    16.     Advisory 17
    17.     Advisory 18
    18.     Advisory 19
  6. 4Silicon Revision A Advisories
    1.     Advisory 01
  7. 5Revision History

Advisory 07

Wrong Reset Source Indication

Revision Affected:

A and B

Details:

The field RESET_SRC in the register AON_SYSCTL:RESETCTL shows the source of the last system reset. Occurrence of one of the reset sources may trigger several other reset sources as essential parts of the system are undergoing a reset. This field will report the source of the reset (not the other resets that are consequence of the system reset). To support this feature, the actual register is not captured before the reset source is released. If a new reset source is triggered within a window of four 32-kHz periods after the previous reset source was released, the register field RESET_SRC may indicate power-on reset as source regardless of the actual reset source.

Workaround:

None