SWRZ143B December 2022 – December 2025 AWRL6432
Incorrect behavior of frame stop API
AWRL6432 ES1.0, ES2.0
The Frame Timer latches Frame Stop command in hardware registers which takes affect at the end of current frame. Frame Stop API issued when Frame Timer has already stopped will result in un-intended stop in the next frame trigger because of the latched stop bit.