SWRZ149B July 2023 – December 2025 IWRL1432
PRODUCTION DATA
Incorrect behavior of frame stop API
IWRL1432 ES1.1, ES2.0
The Frame Timer latches Frame Stop command in hardware registers which takes affect at the end of current frame. Frame Stop API issued when Frame Timer has already stopped will result in un-intended stop in the next frame trigger because of the latched stop bit.