TIDUF29 October 2023
Many of the common device configurations intended for the reference design require configuration through a TI-developed GUI called Latte. This software is required to perform the TX output eye test and the RX link test. The latest version of Latte is available for download by request through TI's website. There are two installation files that the user needs to download and execute: the Latte framework installer file and the Latte libraries updater. As of this publication, the latest Latte installation files are the following:
TI-DS560-Latte_vXpX.exeTI-DS560Lib_vXpX.exeFor detailed instructions on the software installation sequence, functional overview, and initialization sequence for Latte, refer to the software description sections in the DS560DF810 EVM User's Guide. The reference design follows a similar initialization sequence relative to the DS560EVM, with the following key difference: