TIDUF36A May 2023 – December 2023 DRV8328
The sleep mode entry control sub-circuit (shown in Figure 3-11) is used to control the sleep mode entry pin of the DRV8328. When this pin is pulled logic low the device goes to a low-power sleep mode. The control nSLEEP signal from the MSPM0G1507 MCU is used to toggle the sleep mode entry pin with the sub-circuit.
When the signal is pulled logic high, the sleep mode entry pin of the DRV8328 is pulled low and goes into low-power sleep mode. When the signal is pulled logic low, the sleep mode entry pin is pulled high and the DRV8328 remains on.
When J7 is disconnected, nSLEEP can be controlled by the MCU to be at a low level to enter sleep mode. During normal testing, the J7 can be shorted (always nSLEEP enable).