TIDUF60 December 2023
<install_location>\solutions\tida_010265_wminv\f280013x\ccs\motor_controlImport the project within CCS and select the right build configurations by right-clicking on project name as shown in Figure 3-18. Select the right build configuration for the HVAC reference design. The Flash_MtrInv_3SC build configuration supports the three-shunt current sensing method, Flash_MtrInv_1SC supports the single-shunt current sensing method.
Configure the project to select the supporting functions in the project by clicking Project → Import CCS Projects, and browse to <install_location>\solutions\tida_010265_wminv\f280013x\ccs\ for F280013x based reference design, and then right-click on the imported project name, click Properties command to set the pre-define symbols for the project as shown in Figure 3-19.motor_control
Figure 3-18 Select the Correct Build Configurations
Figure 3-19 Select the Correct Predefined Symbols in Project Properties